I cannot log on with a Windows-linked account
Possible cause and solution:
- The number of failed log on attempts exceeded theWindowssecurity policy and theWindowsaccount is temporarily locked.Wait for the lock to expire (typically about 15 minutes), or contact yourWindowsadministrator to enable the account.
- (For systems usingWindows ServerActive Directory Domain Services) There might be authentication problems if your account privileges are assigned usingWindowsgroups that have the Domain Local group scope.Windows-linked groups that reference accounts that are members ofWindowsgroups with Domain Local scope can fail authentication and authorization checks.Add individualWindows-linked accounts explicitly instead of using theWindows-linked group.
- The log on did not include the full user name credential.Try logging on again, making sure to include the domain name with the user name, like this:MyDomain\MyAccountName.Typically, the security system recognizesWindows-linked user credentials without requiring a domain name. However, a domain name is required if:
- You are logged ontoWindowsin one domain, and then attempt to log on toFactoryTalkusing aWindows-linked account that is a member of a different domain. Security is not aware of other domains, so the authentication fails.
- Both aFactoryTalkuser account and aWindows-linked user account have the same user name but different passwords. Security always checks first for a validFactoryTalkuser account. If it finds a matching user name, it attempts to authenticate the account using the password you entered. If the password applies to theWindows-linked user account, authentication fails.
- Both a user account and aWindows-linked user account have the same user name and the same password. Because security always checks first for a validFactoryTalkaccount, if it finds a match, it logs on that user account, and theWindows-linked user account will never be logged on.
- You are currently logged ontoWindowswith user credentials that do not have the necessaryWindowspermissions to access the user information required to log on with a different user account.
How security authenticates user credentials
- Against the list ofFactoryTalkuser accounts. If a match is found, the user is allowed to proceed.
- Against the list ofWindows-linked user accounts. If a match is found, the user is allowed to proceed.
- Against the list of accounts in aWindows-linked user group. If a match is found for the user name and password in aWindows-linked user group, the user is allowed to proceed, even if noWindows-linked user account is present for that user.
If security cannot authenticate the user credentials in the current
Windows
domain or on the local computer, then the logon fails. If using a computer that is part of a different domain then your user account, simply include the domain name with the user name when logging on to FactoryTalk
. Provide Feedback