Remove accounts from a FactoryTalk user group
After creating a
FactoryTalk
user group, members can be added or removed at any time. However, after a Windows
-linked user group is added to the FactoryTalk Directory
, its members cannot be deleted or removed.
TIP:
Alternatively, change the groups to which a user belongs. Use
Group Membership User Properties
to add or remove groups from either a FactoryTalk
or Windows
-linked user account.To remove accounts from a
FactoryTalk
user group- InFactoryTalk Administration ConsoleExplorer, expandSystem>User Groups, right-click the user group account, and selectRemove.
- InSelect User or Group, select each user or user group to remove from the user group account. Use the options underFiltersto show only users, only user groups, or all account.
- SelectOKwhen finished.
Provide Feedback