Add accounts to a FactoryTalk user group
Any time after creating a
FactoryTalk
user group, add or remove the user accounts that belong to the group. Members of a Windows
-linked user group cannot be added or removed. However, individual Windows
-linked user accounts can be added to FactoryTalk
user groups.
TIP:
Alternatively, change the groups to which a user belongs. Use
Group Membership User Properties
to add or remove user groups from a FactoryTalk
or Windows
-linked user account.To add accounts to a
FactoryTalk
user group- InFactoryTalk Administration ConsoleExplorer, expandSystem>User Groups, right-click the user group account, and selectProperties.
- SelectAdd.
- InSelect User or Group, select each user or user group to add to the user group account. Use the options underFiltersto show only users, only user groups, or all accounts. SelectOKwhen finished.
Provide Feedback