Add a FactoryTalk user group
Create a new
FactoryTalk
user group to administer security permissions for specified users as a group. Change the memberships of a user account to quickly change the resources a user can access.A
FactoryTalk
user group can contain:- Windows-linked user group accounts
- LDAP-linked user group accounts
- Cloud-based authentication group accounts
- FactoryTalkuser accounts
- Windows-linked user accounts
Use
New User Group
to add a FactoryTalk
user group account to the FactoryTalk Directory
that is separate from a Windows
user group account. Then specify the group account's identity (for example, the name of the group) and the user accounts that are members of the group. Delete a user group when a particular group account is no longer needed to manage a group of users. Prerequisites
Adding a
FactoryTalk
user group requires these permissions:- Common > Create Children
- Common > List Children
- Common > Read
To add a user group account
- InFactoryTalk Administration ConsoleExplorer, expandSystem>User Groups.
- Right-click theUser Groupsfolder, point toNew, and selectUser Group.
- Type a name for the group in theNamebox.
- (optional) Enter any notes about the group in theDescriptionbox.
- (optional) In theE-mailbox, type only one email address or group address to associate with this group account.
- SelectAddto add user accounts to the group. InSelect User or Group,select to select the users or groups to add to the new user group account. UnderFilter Users, choose from the following:
- Show groups only
- Show users only
- Show all
- Create New
- SelectOKto add the selected user or group to theMembers ListinNew User Group.
- SelectOKwhen finished creating the user group.
Provide Feedback