Log off of FactoryTalk
To log off the current
FactoryTalk Directory
on the current computer, use the Log On to FactoryTalk
tool. Use this tool to log off the current user account and switch to a different user account.
TIP:
If single sign on is enabled, logging off from
FactoryTalk Administration Console
or from another FactoryTalk
product does not log off from FactoryTalk
. To log off from FactoryTalk, either run Log On to FactoryTalk
or log off Windows. To log off of
FactoryTalk
- Double-click theicon in the notification area ofFactoryTalk DirectoryWindowstaskbar. Alternatively, go toRockwell Software >Log On to FactoryTalk.
- InLog On to FactoryTalk, inDirectory, select the directory (NetworkorLocal) to log off from, and selectLog Off. SelectOKto confirm the log off.
- (optional) To log off the other directory, select it inDirectory, and selectLog Off.
- SelectClose.
Provide Feedback