Change logon

Use the
Log On to FactoryTalk
tool to log on to a
FactoryTalk Directory
with another user account. For example, log on to one
FactoryTalk Directory
(network or local) with one user account, and to the other directory with a different user account.
To change logon
  1. Double-click the
    FactoryTalk Directory
    icon in the notification area of
    Windows
    taskbar or start the
    Log On to FactoryTalk
    utility.
  2. In
    Log On to FactoryTalk
    , in
    Directory
    select the directory to log on to (
    Local
    or
    Network
    ).
  3. If currently logged on to the directory, select
    Change Logon
    , if not logged on,
    select
    Logon.
    Log On to
    FactoryTalk
    - (Network or Local)
    appears.
    • If a username and password are required, enter the account
      User name
      and
      Password
      for a default FactoryTalk user, Windows user, or Microsoft Entra ID user, LDAP user group, or OpenID Connect.
    • If a badge is required, tap the badge on the card reader
    • If a badge and password are required, tap the badge on the card reader and then type the password.
      FactoryTalk
      immediately logs in to the selected network with the new user account credentials. The
      Log On to FactoryTalk
      tool displays the account logon details.
  4. Select
    Close
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal