Set up sample demonstrations

The installation process places the
SampleDemo1
and
SampleDemo2
folders in the
FTBatch_Projects
share on the
FactoryTalk® Batch
Server computer. Within each of these
SampleDemo
folders are four subfolders that contain the project data, including area model and recipes.
To set up sample demonstrations:
  1. Add a
    FactoryTalk Security
    user.
  2. Configure the
    FactoryTalk Batch
    Server to locate the area model.
  3. Verify the recipes in the area model.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal