Rebuild the recipe directory

The working set of recipes is stored in the location specified in the
FactoryTalk Administration Console
.
TIP: To set the
Recipe storage
directory, in
FactoryTalk Administration Console
Explorer
right-click an existing server to open the server's properties. If you need to create a server, right-click an application or area name and select
Add New Server
FactoryTalk Batch Server
. Set the
Recipe storage
in the
FactoryTalk Batch Services Properties
dialog on the
Project Settings
tab. In the
Recipe storage
area select the
Recipe Directory
to select the location where you wish to store recipes.
If a recipe has been added to, or deleted from, this recipe storage location without using the
FactoryTalk Batch Recipe Editor
, rebuild the recipe directory.
To rebuild the recipe directory
  1. There are two options:
    • If the
      FactoryTalk Batch Recipe Editor
      is closed, open it to rebuild the recipe directory. Any recipe file additions or deletions are shown when using the
      Open, Remove, Import, Export
      , or
      Generate Reports
      menus in the
      FactoryTalk Batch Recipe Editor
      .
    • If the
      FactoryTalk Batch Recipe Editor
      is already open, select
      File
      Rebuild Recipe Directory
      . The
      FactoryTalk Batch Recipe Editor
      reads all the currently stored recipes and updates the recipe directory file.
  2. If a recipe version conflict occurs when rebuilding the directory, the
    Resolve Version Conflict for Rebuild Recipe Directory Request
    dialog opens. A prompt opens to retain one of the two recipes that conflict.
    TIP:
    If there are unverified recipes in the recipe directory, the option to verify and validate all recipes displays.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal