The eProcedure Server
e
Procedure ServerFor ease of understanding, and for tutorial purposes, this guide refers to configuring and
using the sample files installed with Server, and the
FactoryTalk
Batch. The SampleDemo folders contain complete area models and recipes for a simulated
plant. Before running the demonstrations, you must add a FactoryTalk® Security
user, configure the FactoryTalk Batch
Server to recognize the required project directories, select the initialization path and
file name, and then start the FactoryTalk Batch
Server, the FactoryTalk
e
ProcedureFactoryTalk Batch
Phase Simulator.
TIP:
This guide outlines the configuration and use of the
SampleDemo demonstration files. It is recommended that you follow the directions for using
this demonstration step by step.
The Server provides the services to the Server uses HTTPS. uses OLE for Process Control (OPC) for communications between the Server and the
FactoryTalk
e
ProcedureFactoryTalk Batch
Server to enable the use of HTML instruction files. Communication from FactoryTalk Batch View
to the e
ProcedureFactoryTalk
e
Proceduree
ProcedureFactoryTalk Batch
Server.The Server coordinates the following functions:
e
Procedure- Provides the services to theFactoryTalk BatchServer to enable the use of HTML instruction files.
- Formats parameters and report parameters from material-based recipes into instruction files.
This section assumes that the Server, the
FactoryTalk
e
ProcedureFactoryTalk Batch
Server, and FactoryTalk Batch View
have been installed and configured. [See the for more information.]Provide Feedback