Start the Batch and eProcedure Servers
e
Procedure ServersThe Servers may start automatically when the computer starts. By default the
FactoryTalk Batch
and FactoryTalk
e
ProcedureFactoryTalk Batch
Server starts in production mode. If FactoryTalk Batch
is not activated, run the tutorial in demo mode. While in demo mode, the FactoryTalk Batch
Server runs for a two-hour period and then stops.
TIP:
The
FactoryTalk Batch
Server does not start in production mode without activation. (See the Activate
Rockwell Software Products
insert included with the software CD.)
IMPORTANT:
If you are using
Windows
server to host your FactoryTalk Batch
and eProcedure Server, ensure that the Internet Explorer
Enhanced Security
Configuration setting on the server has been turned off.For instructions, see Microsoft Web site.
To start the Batch and Servers:
e
Procedure- SelectStart, point to , and then selectBatch Service Manager. TheFactoryTalk Batch Service Manageropens.TIP: This procedure requires administrator privileges.
- If theFactoryTalk BatchServer is not already listed in theServicebox, select it from the list.
- If theFactoryTalk BatchServer is running, selectStop.
- If the name of the computer where theFactoryTalk BatchServer is installed does not display in theComputerbox, select theSelect Computerbutton. TheSelect Computerdialog box opens.
- In theEnter the object name to selectarea, type the name of the computer where theFactoryTalk BatchServer is installed (or selectAdvancedto search for a computer). SelectOK.TIP: TheFactoryTalk BatchService Manager must communicate with theWindowsService Manager of the selected computer to determine what services are available. There may be a noticeable delay as communications are established. If the Service Manager cannot communicate with theWindowsService Manager of the selected computer, a message displays.
- From theServicelist, selectFactoryTalk Batch Server.TIP: IfNo Batch Servicesdisplays in the list, theFactoryTalk BatchServer is not installed on the selected computer. See the for instructions.
- To start theFactoryTalk BatchServer in Demo mode, selectAllow Demo Mode.
- Select the method to use for restarting the server.Methods for restarting the serverMethodDescriptionCold RestartTheFactoryTalk BatchServer starts in a new instance without restoring data from its previous run. Batches are not added back to the batch list, and operator arbitration states are not recovered. For all batches that were not restored, batch completion events are recorded in theFactoryTalk BatchEvent Journals. After a Cold Restart, you will not be able to resume execution of batches from the previous instance. If Security Authority is enabled, SAIs in a secured area model and any secured recipes must match the current Network FactoryTalk Directory SAI.Warm RestartRestarts theFactoryTalk BatchServer and attempts to restore the set of batches that were on the batch list when the server previously stopped. Batch complete events are added to theFactoryTalk BatchEvent Journals for all batches that were not restored to the batch list. After a Warm Restart, any batches that are not restored cannot be recovered or resumed in the future. Batches are restored in Manual execution mode with active transitions in a HELD state. No validation for Security Authority is performed.Warm All RestartTheFactoryTalk Batchserver attempts to restart but will not restart if it is unable to restore all the batches to the batch list. If a Warm All Restart attempt fails, the ability to restore batches in the future is not affected. After the issues are resolved, another attempt to restore the batches to the batch list can be made using Warm Restart, Warm All Restart, or Hot Restart. This is the default setting for automatic restarts. Batches are restored in Manual execution mode with active transitions in a HELD state. No validation for Security Authority is performed.Hot RestartFollows all the startup rules of Warm All Restart. In addition, theFactoryTalk BatchServer attempts to restore batches to their last known state, including transition states and recipe modes, without any operator interaction.
- SelectStart/Continue. The Service State area changes from STOPPED to START PENDING. After a few moments, RUNNING displays and the light changes to green.TheFactoryTalk BatchPhase Simulator may start automatically and open a window. If so, minimize the window.
- Select theServer from theeProcedureServicelist.
- Select the method to use for restarting the server.Methods for restarting the serverMethodDescriptionCold Restart - checkedRestarts theFactoryTalkServer in a cold state. All control steps, plus all signatures and previously-entered values associated with the control step due to parameter deviation or cancelled step verification signatures, are removed.eProcedureCold Restart - uncheckedRestarts theFactoryTalkServer, restoring the control steps that were active when the server previously terminated (the control step is restarted with a new reactivation number).eProcedure(See Effects of warm boot on control steps for more information.)
- SelectStart/Continue. TheServer starts running.eProcedure
- ClickCloseto close theFactoryTalk BatchService Manager.TIP: If conversation becomes LOST while running in Demo mode, make sure that the Simulator is running and try starting the server(s) again. SeeStart the FactoryTalk Batch Phase Simulatorfor more information.
Provide Feedback