Start the sample FactoryTalk Batch Phase Simulator
FactoryTalk Batch
comes with a phase logic simulation program, referred to as the
FactoryTalk Batch
Phase Simulator used to simulate the batch process without
connecting to a PCD. The Phase Simulator imitates the functionality of a data server and can
communicate with the FactoryTalk Batch
Server using OPC communication protocol. The
Phase Simulator is a powerful tool for testing, experimentation and demonstration purposes.
In this guide, run the sample demonstration using the Phase Simulator.
TIP:
If the Phase Simulator is required and OPC protocol is used for communications, the
FactoryTalk Batch
Server automatically starts the Phase Simulator. Check the
Windows taskbar to see if the Phase Simulator is started.To run the sample demonstration correctly, open the
ice_cream1.sim
file in the Phase Simulator. Start the sample
FactoryTalk Batch
Phase Simulator:- If the Phase Simulator is already running, maximize it from the Windows taskbar. If the Phase Simulator is not running, select . TheFactoryTalk BatchPhase Simulator opens.TIP: This procedure requires administrator privileges.
- Select . TheOpen Simulator Configuration Filedialog opens.
- From theLook inlist, open the folder. Select theice_cream1.simfile, and then selectOpen.
- Minimize theFactoryTalk Batch Phase Simulatorwindow.
Provide Feedback