Search
PointMax Dual Stepper Drive Module
Motor and Axis Configuration
This chapter describes the axis features of the stepper module and how to configure the parameters.
Stepper Motor Compatibility
Scaling
Invert Direction
Axis On and Off State
Velocity Profiles
Home Operation
Modes and Commands
Overtravel Detection
Motor Torque Off
Motor Brake
Axis Behavior at Program Mode, Inhibited, or Communication Fault Mode
Axis Fault Reporting
Reconfiguration
Provide Feedback
Have questions or feedback about this documentation? Please
submit your feedback here
.
Normal