Axis Fault Reporting
The axis sets the I.Axisxx.Fault tag when it detects a fault.
The following faults are latched:
- Short Circuit
- Critical Temperature
- Motor Torque Off
- Field Power Loss
- Brake Faulted
To clear a latched fault, do the following:
- Remove the cause of the fault.
- Trigger a rising edge on O.Axisxx.ResetFault to clear I.Axisxx.Fault and the corresponding fault bit.
- When a Short Circuit, Critical Temperature, Motor Torque Off, or Field Power Loss fault occurs, the axis is disabled. You must trigger a rising edge on O.Axisxx.Enable to re-enable the axis.
Axis Fault Detection and Recovery Timing Diagram
Provide Feedback