Axis Behavior at Program Mode, Inhibited, or Communication Fault Mode

When the module is inhibited, transitions to Program Mode, or enters the Communication Fault state, the axis is disabled (powered off).
When in Program Mode, the module clears the I.Axisxx.BrakeReleased tag immediately so that the external brake can be applied.
When the module is inhibited, or a communication fault exists, the controller clears the I.Axisxx.BrakeReleased tag immediately so that the external brake can be applied.
IMPORTANT: The axis might still be decelerating when the brake is applied. To help avoid this issue, always disable the axis (clear O.Axisxx.Enable) before you inhibit the module or enter Program Mode.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal