Invert Direction
You can configure the axis to move in the opposite direction using the tag
C.Axisxx.InvertDirection. This function is useful if the axis is being transferred to
the opposite side of the load and can be achieved by only changing the configuration
instead of changing the ladder application program.
Direction | C:InvertDirection = 0 | C:InvertDirection = 1 |
|---|---|---|
Forward direction | ![]() Clockwise | ![]() Counterclockwise |
Reverse direction | ![]() Counterclockwise | ![]() Clockwise |
Provide Feedback