Search
PointMax 4-Channel IO-Link Master Module
IO-Link Device Integration
This chapter describes the common features that are available with IO-Link integration in the Studio 5000 Logix Designer application.
IO-Link Device Identity
IO-Link Bus
IODD-based AOP for IO-Link Devices
Fallback Mode
IO-Link Device Connection
IO-Link Device Inhibiting
IO-Link Device Electronic Keying
Automatic Device Configuration
Data Storage
IO-Link Device Parameters Classification
Device Configuration
Device Correlation Check
Get/Set IO-Link Device Parameters
Configure IO-Link Process Data Output State When IO-Link Device is in Program Mode or Inhibited
Configure IO-Link Process Data Output State in Fault Mode
IO-Link Device Information and Diagnostics
Fault and Status Reporting
IO-Link Device Configuration Change Notification
Execute IO-Link Commands Through Explicit Messaging
Protection Mode for IO-Link Devices
IO-Link Events
Register IO-Link Device IODD
Import/Export IODD Files
Use Generic IO-Link Device Profile
Update Device Firmware
Provide Feedback
Have questions or feedback about this documentation? Please
submit your feedback here
.
Normal