Get/Set IO-Link Device Parameters
You can use the Parameters view to retrieve or set the parameters in the IO-Link
device.
- You can retrieve the value of all parameters in the device, including configuration parameters.
- You can set non-configuration read/write parameters.
- You can issue IODD-defined commands that are specific to that IO-Link device to the device in the Parameters view.
Provide Feedback