IO-Link Device Parameters Classification
IO-Link device parameters are classified into two categories:
- Configuration parametersFor devices that support Data Storage, configuration parameters are read/write parameters that are defined in the IODD, which are not excluded from Data Storage.For devices that do not support Data Storage, read/write parameters that are defined in the IODD are configuration parameters.
- Non-configuration parametersAll parameters that are defined in the IODD that do not match the conditions that are defined under configuration parameters are non-configuration parameters.
The Configuration view and the Parameters view of the IO-Link device Module Properties
window are used to handle device parameters.
Only configuration parameters are shown in the Configuration view. Configuration
parameters can only be changed in the Configuration view. The Configuration view only
shows the project values of the configuration parameters.
Use the Parameters view to access non-configuration parameters and retrieve device values
of configuration parameters. All parameter values that are shown in the Parameters view
are device values.
Provide Feedback