Device Correlation Check

Use the Device Correlation Check feature to synchronize the Studio 5000 Logix Designer application project and IO-Link device copies of the configuration parameters values. You can use this feature to back up the configuration parameters from the IO-Link device to the project, or to restore the configuration parameters from the project to the device.
When ADC is enabled:
  • The project values are synchronized to the device automatically when connection is established.
  • The project values are stored in the configuration tags and are visible to the ladder program.
When ADC is disabled:
  • The project values are only accessible through the IO-Link device properties. You must apply the configuration or perform Device Correlation Check to synchronize the project values and device values.
  • Device Correlation Check is automatically performed when the Configuration view is opened.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal