IODD-based AOP for IO-Link Devices
Every IO-Link device has its own Add-on Profile (AOP) in the Studio 5000 Logix Designer
application project. The features that are available in the IO-Link Device Description
(IODD) are integrated into the AOP.
Once the IODD for the device is registered, you can add the device under the IO-Link bus,
where you can access the device Module Properties window to define/control connections,
configure, and monitor the status of the device.
To register the IODD for your device, see Register IO-Link Device IODD and Import/Export IODD Files.
Provide Feedback