Develop Secure Applications
The following controllers support IEC-62443-4-2 SL 1 security certification.
Controller | Firmware Revision |
|---|---|
ControlLogix® 5580 standard controllers | 32 or later |
ControlLogix® 5580 NSE, XT, K, and Process controllers | 33 or later |
GuardLogix® 5580 controllers | 37 or later |
IMPORTANT:
If enabled, the following features cause the controller to be excluded from IEC-62443-4-2 SL 1 security certification:
- OPC UA
- Redundancy
- Secure socket objects
- Remote deployment of save/restore images
To help meet these requirements, you must use this publication and the Configure System Security Features User Manual, publication SECURE-UM001. The Configure System Security Features User Manual describes how to configure and use
Rockwell Automation®
products to improve the security of your industrial automation system. The controller accepts all values appropriate for a tag data type, and it is the responsibility of the user program to specify valid ranges and perform validity to check for those ranges. The controller verifies incoming messages for syntax, length, and format.
You can apply these same measures to other
ControlLogix®
and GuardLogix®
controllers, but without security certification.Resource | Description |
|---|---|
Security Design Guide Reference Manual, publication SECURE-RM001 | Provides guidance on how to conduct vulnerability assessments, implement Rockwell Automation® products in a secure system, harden the control system, manage user access, and dispose of equipment. |
Logix 5000 Controllers Security Programming Manual, publication 1756-PM016 | Describes how to configure security for the Studio 5000 Logix Designer® application, and explains how to configure source protection for your logic and projects. |
CIP Security Application Technique, publication SECURE-AT001 | Describes how to plan an implement a Rockwell Automation® system that supports the CIP Security™ protocol. |
Converged Plantwide Ethernet (CPwE) Design and Implementation Guide, publication ENET-TD001 | Defines manufacturing-focused reference architectures to help accelerate the successful deployment of standard networking technologies and convergence of manufacturing and enterprise/business networks. |
Provide Feedback