Disable Controller Webpages via Controller Properties

You can use one of the following methods to disable the controller webpages:
  • If the controller web pages are enabled, disable them by clearing the Enable Controller Web Pages check box on the Security tab for the controller properties.
    This image shows how to enable and disable controller web pages via Logix Designer properties dialog box.
    IMPORTANT:
    In version 36 or later, the status of the Enable Controller Web Pages checkbox is saved to and restored from the memory card when using the save/restore feature.
    Previous versions maintain the status of the Enable Controller Web Pages checkbox that was applied to the controller prior to a restore from the memory card.
  • For
    CIP Security
    applications, you can also use
    FactoryTalk® Policy Manager
    to disable the webpages (this overrides the Controller Properties checkbox).
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal