Disable the Controller USB Port

With the
Studio 5000 Logix Designer®
application, version 32 or later, you can use a
CIP
Generic MSG with a Path of THIS to execute this option.
  1. Add an MSG instruction to your program.
    This message only has to execute once, it does not need to execute with every program scan.
    IMPORTANT:
    You cannot add an MSG instruction to your program if the controller switch is in Run mode, or if the
    FactoryTalk® Security
    settings deny this editing option.
  2. Configure the Configuration tab on the Message Configuration dialog box as described in the table below.
    This image shows how to configure the MSG instruction that disable a controller's USB port in Logix Designer.
    IMPORTANT:
    These values are stored to non-volatile controller memory in such a way that the MSG instruction is not required to execute up each time the controller powers up.
    Disable the USB Port
    Field
    Description
    Message Type
    CIP Generic
    Service Type
    Set Attribute Single
    Instance
    1
    Class
    33a
    Attribute
    4
    Source Element
    Controller tag of SINT data type.
    In this example, the Source Element is named Port_Configuration.
    Source Length
    1
  3. Configure the Communication tab to use a Path of THIS.
    IMPORTANT:
    Messages to THIS must be unconnected messages.
    This image shows an example of how to configure the Comm path to disable a controller's USB port in Logix Designer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal