Controller Webpage Default Settings

The following are the default settings for controller webpages:
  • Webpages are enabled for controller firmware revision 32 or earlier. You must reconfigure the settings to disable the controller webpages after it returns to its default settings.
  • Webpages are disabled for controller firmware revision 33 or later. You must reconfigure the settings to enable the controller webpages after it returns to its default settings.
Controller webpages return to the default setting in these situations:
  • A stage 1 reset for all versions of the
    Studio 5000 Logix Designer®
    application.
  • A stage 2 reset for all versions of the
    Studio 5000 Logix Designer®
    application.
    IMPORTANT:
    When you update the controller firmware to revision 33 or later without a reset, the controller retains the previous controller webpage configuration (webpages enabled) and does not automatically change to the default setting for version 33 (disable the webpages).
The setting of the controller webpages changes after the following occurs on the controller:
  • New project is downloaded - in this case, the settings in the new project take effect.
  • When the controller receives a configuration message, it takes the setting from the configuration message.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal