Settings screen
How do I open the Settings screen?
On the physical HMI device or in the System Banner at the top of the screen, press
and then tap
Navigation
and then tap Settings
.Use the
Settings
screen to view and change HMI device and system-wide settings. On the Settings
screen, select an option to perform its related tasks:Option: | Popup: | Tasks: |
Network | NetworkIPSettings tab |
|
NetworkLinkSettings tab |
| |
NetworkDiagnostic tab | View network diagnostics | |
Display | Display |
|
HMI Device | HMIDevice |
|
HMIDevice_RebootConfirm | Reboot the HMI device | |
Data Export | Data Export |
|
Troubleshooting | Troubleshooting |
|
Date and Time | DateAndTime |
|
Controllers | ControllersGeneral tab | View controller reference and status information |
ControllersDiagnostic tab | View controller diagnostics | |
Load from Media | Load Application | Load a .vpdr file from an USB storage device or an SD Card inserted into the HMI device. |
VNC | VNC | Enable View-Only or Full-Control access rights or disable remote VNC connection. |
Email | Email | Configure the connection to an email server enable sending emails when a Send Email command executes on the HMI device. |
Certificate | Certificate | Import digital certificates from removable media to gain secured access to resources on the Internet or delete digital certificates you no longer need from the HMI device. |
Provide Feedback