Reboot the HMI device
Reboot the HMI device to run the current project again. Data logs in the project remain unchanged when rebooting the HMI device. The data log starts collecting data again after the reboot completes.
To reboot the HMI device
- On the HMI device or in theSystem Banner, selectNavigation
and then select Settings. - SelectHMI Device. TheHMI Devicepopup opens.
- SelectReboot. A prompt appears to confirm rebooting the HMI device.
- SelectYesto reboot the HMI device. SelectNoto not reboot the HMI device. Rebooting the HMI device opens the currently downloaded project.
Provide Feedback