Add-On Graphic tab
How do I open the Add-On Graphic tab?
In the
Project Explorer
, expand the Assets
and Add-On Graphics
folders to navigate to the Add-On Graphic and then perform one of the following:- Double-click the Add-On Graphic.
- Right-click the Add-On Graphic and then selectOpen.A tab with the name of the Add-On Graphic opens.
The
Add-On Graphic
tab displays the definition of an Add-On Graphic. The definition includes:- Graphic elements contained in the Add-On Graphic.
- Property values, animations, and events of graphic elements contained in the Add-On Graphic.
- User-defined properties for the Add-On Graphic.
Use the
Add-On Graphic
tab to: - Display the content of the Add-On Graphic.
- Add a graphic element to or remove a graphic element from the Add-On Graphic.
- Move, flip, or rotate a graphic element in the Add-On Graphic.
- Change property values for the Add-On Graphic.
- Change property values for a graphic element in the Add-On Graphic.
- Change property definitions for the Add-On Graphic.
- Add animations or events to a graphic element in the Add-On Graphic.
Provide Feedback