Open the definition of an Add-On Graphic

Open the definition of an Add-On Graphic to add or change the content of the Add-On Graphic. For example, change the property values of graphic elements, the property definitions of the Add-On Graphic, or the behavior of the content of an Add-On Graphic.
To open the definition of an Add-On Graphic
  1. In the Project Explorer, expand the
    Assets
    and
    Add-On Graphics
    folders.
  2. Right-click the Add-On Graphic and select
    Open
    . You can also double-click the Add-On Graphic. The definition of the Add-On Graphic opens in a separate tab.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal