Change property values for a graphic element in the definition of an Add-On Graphic
Change the properties for a graphic element in the definition of an Add-On Graphic to change the appearance of only that graphic element.
To change property values for a graphic element in the definition of an Add-On Graphic
- In the Project Explorer, expand theAssetsandAdd-On Graphicsfolders.
- Double-click the Add-On Graphic. The definition of the Add-On Graphic opens in a separate tab.
Select the graphic element in the Add-On Graphic. The properties for the selected graphic element appear in theTIP:Tips:- Right-click the Add-On Graphic and selectOpenor pressEnterwhen the Add-On Graphic is selected to open the definition.
- If an instance of the Add-On Graphic exists on a screen, right-click the Add-On Graphic on the screen or in theGraphic Explorerand then selectOpen Graphic Definitionto open the definition. TheOpen Graphic Definitionoption is unavailable for selected groups and multiple selected graphic elements, even if the selection contains an Add-On Graphic.
Propertieswindow.- In thePropertieswindow, change the property values.TIP:If a graphic element with an aliased property in the definition of an Add-On Graphic is unlinked, the unlinked property is not changed in the instances of the Add-On Graphic.
Provide Feedback