Close the definition of an Add-On Graphic
Close an Add-On Graphic like any other screen when changes to the definition of the Add-On Graphic are complete.
To close the definition of an Add-On Graphic
- On the tab of the open Add-On Graphic definition, selectClose
.
Provide Feedback