Navigation menu
How do I open the Navigation menu?
On the HMI device, tap
in the press
Navigation
in the System Banner
at the top of the screen,Alt/n
on an external keyboard, or press the physical Navigation
button on the HMI device. Use the
Navigation menu
to navigate to and open shortcuts to screens created in Studio 5000
View Designer
. The Navigation menu
on the HMI device displays the contents of the Navigation Menu
folder in the Project Explorer
of Studio 5000
View Designer
. The Navigation menu
appears at the bottom or left side of the HMI device screen. The menu items displayed in the
Navigation menu
depend on the security access granted to the security role assigned to the logged on user. Security is set in Studio 5000
View Designer
. If assigned the Operator role, the Navigation menu
displays only the items to which the Operator has access. Provide Feedback