Specify a Home screen
The
in the
Home
screen is the initial screen that opens when the HMI device starts. For a new project, the default Home
screen is Screen_001. The Home
iconNavigation Menu
folder of the Project Explorer
indicates that Screen_001 is the Home
screen. Screen_001 in the Navigation Menu
folder of the Project Explorer
is a shortcut based on Screen_001 in the User-Defined Screens
folder. Designate any shortcut in the Navigation Menu
folder as the Home
screen of the project. To specify a Home screen
- In theProject Explorer, expand theNavigation Menufolder.
- Right-click the shortcut and selectSet as Home. TheHomeicon
appears next to the shortcut. This is the Homescreen that opens automatically when the HMI device restarts.
Provide Feedback