Omit an item from the Navigation menu
By default, all shortcuts and folders in the
Navigation Menu
folder of the Project Explorer
are represented as items in the Navigation menu
on the HMI device.Navigation menu
on the HMI device by deleting it from the Navigation Menu
folder. Do this if a screen in a project depicts a line in your system that is no longer in production. Deleting the shortcut designated as the Home
screen for a project is not allowed. You cannot delete the shortcut with the Home
icon Navigation Menu
folder. Prerequisites
- To delete a shortcut designated as theHomescreen of the project, designate a new shortcut as theHomescreen.
To omit an item from the Navigation menu
- In theProject Explorer, expand theNavigation Menufolder.
- Right-click the shortcut and selectDelete. The shortcut no longer appears in theNavigation Menufolder or theNavigation menuon the HMI device.TIP:Have an item not appear in theNavigation menuby restricting access to the item. Only items to which the assigned user role has access appear in theNavigation menuon the HMI device.
Provide Feedback