System

The
System
category in the
Toolbox
contains graphic elements used in the system by default. Some of the graphic elements in this category are elements without built-in animation properties. Other graphic elements in this category are pre-configured to perform a task. The graphic elements in
System
are organized into categories:
  • Activity Indicator
  • Alarm Status Indicator
  • Checkbox
  • Controller Status Indicator
  • Error
  • List Box Indicator
  • List Box Selector
  • Navigation Menu
  • Network Status Indicator
  • PDF Viewer
  • Radio Button
  • Success
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal