Controller Status Indicator
The Controller Status Indicator is a graphic element pre-defined to show controller communication issues and open the screen for configuring controllers. This graphic element appears in the
System
category of the Toolbox
. Use the Controller Status Indicator to:
- See a visual indicator when there is an issue with the communication of any controller in the project.
- Open theControllerspopup. This popup shows details about the communication status of all referenced controllers in the project.
- Change the screen the Controller Status Indicator opens. When selecting the Controller Status Indicator, change the screen name in theNavigateTobox of thePropertieswindow.TIP:Tips:
- By default, the Controller Status Indicator appears in theSystem Bannerat the top of the screen. The same controller details appear when selectingControllerfrom theSettingsscreen.
- The Controller Status Indicator changes appearances based on the issue:
Controller error.Any controller in the project has no power or connection.
Controller caution.Any controller in the project has a fault or is inProgrammode.
Controller unknown.No controller is visible or it is unclear if a controller should be visible to the HMI device. This occurs when any controller referenced in the project is disconnected, powered down, or is on a disconnected side of the network.
Built-in Animation Properties
Built-in animation properties appear under the
General
category of the Properties
window. Specify values for these properties in order to animate the graphic element or change the information the graphic element shows on the HMI device. Name | Category | Purpose | Accepted values |
NavigateTo | General | Specifies the screen to open on a touch release event. | Screen name in project |
Common properties exist for all graphic elements.
Property | Category | Purpose | Accepted Values |
Access | Security | Specifies if all users have access to the control element, or if access is inherited from the screen. |
|
Angle | Position and Size | Specifies the rotation angle. Enter 180 to display the graphic element upside down. If you enter a value larger than 360, the portion of numeric value that is over 360 becomes the value. For example, enter 380 to see a value of 20. If you enter a value less than 0, the negative value is subtracted from 360. For example, enter -30 to see a value of 330. |
|
Enabled | Appearance | Specifies if the graphic element is available on the HMI device and if the graphic element accepts touch and key input. |
|
Height | Position and Size | Specifies the height in pixels. | Any positive numeric value |
Opacity | Appearance | Specifies the transparency of the graphic element. | 0 (fully transparent) - 100 (fully opaque) |
Visible | Appearance | Specifies if the graphic element is visible on the HMI device. |
|
Width | Position and Size | Specifies the width in pixels. | Any positive number |
X | Position and Size | Specifies the horizontal coordinate, in pixels, from the upper left corner of screen to the upper left corner of a graphic element or group with no rotation. If the graphic element or group is rotated, the X property value does not change. | Any positive number |
Y | Position and Size | Specifies the vertical coordinate, in pixels, from the upper left corner of screen to the upper left corner of a graphic element or group with no rotation. If the graphic element or group is rotated, the Y property value does not change. | Any positive number |
Provide Feedback