Alarm Status Indicator
The
is pre-defined to open the
Alarm Status Indicator
button
is pre-defined to open the Alarm Summary
screen. This graphic element appears in the System
category of the Toolbox
. Use the
Alarm Status Indicator
to:- Open theAlarm Summaryscreen on the HMI device. By default, this button opens theAlarmSummaryscreen.
- Change the screen the Alarm Status Indicator opens. With the Alarm Status Indicator selected, change the screen name in theNavigateTobox of thePropertieswindow.TIP:Tips:
- AnAlarm Status Indicatorbutton appears in theSystem Bannerat the top of each screen. The button is red and flashing when there are active alarms that are unacknowledged.
- The button remains red as long as there are active alarms (acknowledged or unacknowledged).
- The button returns to default state with gray icon when all alarms are normal, even if alarms are unacknowledged.
Built-in animation properties
Built-in animation properties appear under the
General
category of the Properties
window. Specify values for these properties in order to animate the graphic element or change the information the graphic element shows on the HMI device. Name | Category | Purpose | Accepted values |
NavigateTo | General | Specifies the screen to open on a touch release event. | Screen name in project |
Common properties exist for all graphic elements.
Property | Category | Purpose | Accepted Values |
Access | Security | Specifies if all users have access to the control element, or if access is inherited from the screen. |
|
Angle | Position and Size | Specifies the rotation angle. Enter 180 to display the graphic element upside down. If you enter a value larger than 360, the portion of numeric value that is over 360 becomes the value. For example, enter 380 to see a value of 20. If you enter a value less than 0, the negative value is subtracted from 360. For example, enter -30 to see a value of 330. |
|
Enabled | Appearance | Specifies if the graphic element is available on the HMI device and if the graphic element accepts touch and key input. |
|
Height | Position and Size | Specifies the height in pixels. | Any positive numeric value |
Opacity | Appearance | Specifies the transparency of the graphic element. | 0 (fully transparent) - 100 (fully opaque) |
Visible | Appearance | Specifies if the graphic element is visible on the HMI device. |
|
Width | Position and Size | Specifies the width in pixels. | Any positive number |
X | Position and Size | Specifies the horizontal coordinate, in pixels, from the upper left corner of screen to the upper left corner of a graphic element or group with no rotation. If the graphic element or group is rotated, the X property value does not change. | Any positive number |
Y | Position and Size | Specifies the vertical coordinate, in pixels, from the upper left corner of screen to the upper left corner of a graphic element or group with no rotation. If the graphic element or group is rotated, the Y property value does not change. | Any positive number |
Provide Feedback