Navigation Menu
The Navigation Menu is a button pre-defined to open the
Navigation menu
on the HMI device. This graphic element appears in the System
category of the Toolbox
.Use the Navigation Menu graphic element to:
- Open theNavigation menuat the bottom of the HMI device screen.
- Display only those items to which the logged on user or Guest user has security access.
Unique properties
Unique properties are properties that not all graphic elements in the
Toolbox
share. Name | Category | Purpose | Accepted values |
|---|---|---|---|
CornerRadius | Appearance | Specified the curve of the corners | 0 for a positive number |
Color | Appearance/Border | Specifies the color of the border | Any selected color in the Color Picker or a Hex color value entered manually. The Hex value must be in the format #RRGGBB. R, G, and B are Hex digits from 0 through F and represent the color channel values for red, green, and blue. For example, #ffff00 produces yellow. |
Style | Appearance/Border | Specifies the style of the border line. |
|
Width | Appearance/Border | Specifies the width of the border line. |
|
FillColor | Appearance | Specifies the fill color. | Any selected color in the Color Picker or a Hex color value entered manually. The Hex value must be in the format #RRGGBB. R, G, and B are Hex digits from 0 through F and represent the color channel values for red, green, and blue. For example, #ffff00 produces yellow. |
UsePredefinedDisabled | Appearance | Specifies if a crosshatch overlay shows on the control element when you disable the element. |
|
Common properties
Common properties exist for all graphic elements.
Property | Category | Purpose | Accepted Values |
Access | Security | Specifies if all users have access to the control element, or if access is inherited from the screen. |
|
Angle | Position and Size | Specifies the rotation angle. Enter 180 to display the graphic element upside down. If you enter a value larger than 360, the portion of numeric value that is over 360 becomes the value. For example, enter 380 to see a value of 20. If you enter a value less than 0, the negative value is subtracted from 360. For example, enter -30 to see a value of 330. |
|
Enabled | Appearance | Specifies if the graphic element is available on the HMI device and if the graphic element accepts touch and key input. |
|
Height | Position and Size | Specifies the height in pixels. | Any positive numeric value |
Opacity | Appearance | Specifies the transparency of the graphic element. | 0 (fully transparent) - 100 (fully opaque) |
Visible | Appearance | Specifies if the graphic element is visible on the HMI device. |
|
Width | Position and Size | Specifies the width in pixels. | Any positive number |
X | Position and Size | Specifies the horizontal coordinate, in pixels, from the upper left corner of screen to the upper left corner of a graphic element or group with no rotation. If the graphic element or group is rotated, the X property value does not change. | Any positive number |
Y | Position and Size | Specifies the vertical coordinate, in pixels, from the upper left corner of screen to the upper left corner of a graphic element or group with no rotation. If the graphic element or group is rotated, the Y property value does not change. | Any positive number |
Provide Feedback