Convert a legacy tag database
You must have
FactoryTalk View Studio
, or FactoryTalk SE HMI Server installed on an 64-bit Windows operating system to convert a legacy tag database.To convert a legacy tag database
- Copy the legacy project folder containing the CSV files from the 32-bit Windows operating system to the 64-bit Windows operating system.
Provide Feedback