Legacy Tag Database Conversion utility
How do I open the Legacy Tag Database Conversion utility?
- From WindowsStartmenu, selectAll apps > Rockwell Software > Legacy Tag Database Conversion.
If you are using one of the following products:
- FactoryTalk View SE6.0 or earlier
- RSView32
And you want to upgrade to
FactoryTalk View
6.1 or later on a 64-bit Windows operating system, use the Legacy Tag Database Conversion utility to convert legacy tag database to a new format before you open your legacy applications.If you want to upgrade to
FactoryTalk View
6.1 or later on a 32-bit Windows operating system, you do not need to use this utility. Opening or importing the applications with FactoryTalk View 6.1 or later on a 32-bit Windows operating system automatically converts your tag databases.Provide Feedback