Select the application when exporting the legacy tag databases from a 32-bit Windows operating system

After selecting
Export Legacy Tag Database
, select the application to be converted.
To select the application when exporting the legacy tag databases from a 32-bit Windows operating system
  1. Select the application type you want to convert.
  2. Enter or select the directory for the projects. Click the
    Browse
    button ([...]) to browse for the directory containing the projects.
  3. Select
    Search sub-folders
    to search for projects in the sub-folders of the project folder.
  4. Click
    Next
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal