Select the application when creating the tag databases in new format on a 64-bit operating system

After selecting
Create FactoryTalk View Tag Database in new format
, select the application type that you want to convert.
To select the application type when creating the tag databases in new format on a 64-bit operating system
  1. Select the application type.
  2. Enter or select the directory for the projects. Click the browse button ([...]) to browse for the directory containing the projects.
  3. Select
    Search sub-folders
    to search for projects in sub-folders of the project folder.
  4. Click
    Next
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal