Select the projects to create the tag databases in new format on a 64-bit operating system

After selecting the application type, select the projects to create the tag databases in new format on a 64-bit operating system.
To select the projects to create the tag databases in new format on a 64-bit operating system
  1. Select the projects you want to convert from the list. Click
    Select All
    to select all projects. Click
    Clear All
    to clear all projects.
    TIP:
    Projects that are unavailable have already been converted to FactoryTalk View 6.1 or later.
  2. Click
    Finish
    to begin converting the selected projects.
The utility converts the selected tag databases. When the conversion is finished, the utility shows the log file for the conversion.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal