Application Documenter

How do I open Application Documenter?
  • From Windows
    Start
    menu, select
    All apps > Rockwell Software > Application Documenter
    .
Application Documenter is a stand-alone utility that provides detailed information on
FactoryTalk View
applications. This utility is a browser that allows you to view the contents of the application's components and the tags used in these components. You can also print and export the information.
The left pane of the Application Documenter main window shows the list of components for you to choose from. The right pane contains detailed information for the selected component.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal