Menu options

This section contains the following information:
  • Open Application
  • Close Application
  • Export...(File menu)
  • Log On
  • Log Off
  • Print...(File menu)
  • Print Preview
  • Print Setup...(File menu)
  • Recent Applications (File menu)
  • Exit (File menu)
  • Find (On this Page) - (Edit menu)
  • Toolbar (View menu)
  • Status Bar (View menu)
  • Help Topics (Help menu)
  • About FactoryTalk View Application Documenter... (Help menu)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal