View component information
Use the left pane of the Application Documenter main window to choose the component(s) for which you want more information. You can then view the information for the selected component(s).
To view information about a component
- Open the folder where the component is located.
- Click a component to select it for viewing. The contents of the selected component appear in the right pane.TIP:When you highlight the selected component, the contents appear in the right pane. The highlighted component is also known as the current component.
Provide Feedback