Print component information

You can print the component information to a printer.
To print the component information
  1. Select the check box beside the component(s) whose information you want to print.
  2. From the
    File
    menu, select
    Print
    , or click the
    Print
    toolbar button.
  3. In the
    Print
    dialog box, choose the printer, the range of pages you want to print, and the number of copies.
  4. Click
    OK
    to print. To exit without printing, click
    Cancel
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal