FactoryTalk View Site Edition Client Wizard
How do I open the
FactoryTalk View
Site Edition Client Wizard?
To open the
FactoryTalk View
Site Edition Client Wizard, do one of the following:- SelectStart > Rockwell Software >.FactoryTalk ViewSite Edition Client
- InFactoryTalk View Studio, when you have aFactoryTalk View SEapplication open, from the menu, selectTools>Launch SE Client.
Use the
FactoryTalk View
Site Edition Client Wizard to create a client configuration file, edit or run an existing client configuration file.Provide Feedback