Start an application automatically on a MobileView terminal or a personal computer using parameters
On a
MobileView
terminal or a personal computer, you can start FactoryTalk View ME Station
and runs an application automatically whenever the terminal or computer starts by setting up the startup options or using parameters.To start an application automatically when a
MobileView
terminal or a personal computer starts- Copy the path to the MERuntime.exe file (FactoryTalk View ME Station) to the WindowsStartupfolder.The default folders of the path to the MERuntime.exe file isC:\ProgramData\Microsoft\Windows\Start Menu\Programs\Rockwell Software\.FactoryTalk ViewThe WindowsStartupfolder isC:\Users\<logged in user name>\AppData\Roaming\Microsoft\Windows\Start Menu\Programs\Startup.TIP:If you copied the path to the MERuntime.exe file to the WindowsStartupfolder, to disable the automatic startup ofFactoryTalk View ME Station, delete the file in the Windows Startup folder.
- In theStartupfolder, right-clickFactoryTalk View ME Stationand selectProperties.
- On theShortcuttab, in theTargetbox, after the existing text, type a space, the path to the .mer file, and one or more parameters.For example, to start FactoryTalk View ME Station and open an application calledMalthouse, type"C:\Users\Public\Public Documents\RSView Enterprise\ME\Runtime\malthouse.mer" /r /d /o
- ClickOK.
In the future, whenever the
MobileView
terminal or the personal computer starts, FactoryTalk View ME
Station will start automatically, delete the applications log files, overwrite the terminal's communications file, and run the application.If you do not want to delete the log files, omit the
/d
parameter.If you do not want to overwrite the communications file, omit the
/o
parameter.To give the user the choice of overwriting the communications file, use the
/a
parameter instead of the /o
parameter.Provide Feedback