Stop a runtime application
You may need to stop a runtime application. When the application closes, the runtime system also stops.
To stop a runtime application, do one of the following
- Press a shutdown button on a graphic display.
- Click the close button in the right corner of the title bar. To use this method, select theTitle baroption in theProject Settingsdialog box.
Provide Feedback