Log on to Network Server

If your application is running on a
PanelView Plus
family terminal and is using a shared network drive to store data log files, the
Logon to Network Server
dialog box opens when your runtime file loads. Type your username, password, and the network domain name. What these values are depends on your network. If you are unsure, check with your network administrator.
This information is stored in RAM, and is erased when the machine restarts. Therefore, the information has to be re-entered each time the terminal starts. Selecting the
Update Default Credentials
checkbox will save the network configuration information.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal